i2s format and PCM format

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i2s format and PCM format

跳至解决方案
30,311 次查看
jamesdeepu
Contributor II

Can someone explain what is the difference between I2S interface and PCM interface. Does I2S interface only supports i2s format audio data and not PCM format audio data ?

标签 (3)
标记 (5)
1 解答
9,556 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Basically : I2S is interface, PCM is a digital representation of an audio signal.
"I2S, also known as Inter-IC Sound, Integrated Interchip Sound, or IIS, is an electrical serial bus
interface standard used for connecting digital audio devices together. It is used to communicate PCM
audio data between integrated circuits in an electronic device."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
9,557 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Basically : I2S is interface, PCM is a digital representation of an audio signal.
"I2S, also known as Inter-IC Sound, Integrated Interchip Sound, or IIS, is an electrical serial bus
interface standard used for connecting digital audio devices together. It is used to communicate PCM
audio data between integrated circuits in an electronic device."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

9,556 次查看
jamesdeepu
Contributor II

Dear Yuri,

Thanks for your reply.!!..

So there is nothing like PCM interface ?

Can you explain I2S audio format too?

Thanks in advance.

0 项奖励
回复
9,556 次查看
Yuri
NXP Employee
NXP Employee

Hi,

Please look at sections 3.1 (General PCM Codec)  and 3.2 (I2S) of the following

app note :

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2979.pdf

Regards,

Yuri.

0 项奖励
回复