i2c probe Command Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i2c probe Command Issue

1,834件の閲覧回数
anshulkhare
Contributor III

Hello All,

i am working on IMX6ul board, in u-boot i2c Command is enabled,

but when i am giving i2c probe command through command line i am not getting all the valid chip address,

in logs i am receiving failure continuously.

Valid chip addresses  :

wait_for_sr_state : failed sr=81 cr=a0 state=2020

i2c init transfer : failed for chip 0xx0 retry=0

i am not getting why this failure is coming. 

Could anyone kindly provide us with some information on this. Any help on this is much appreciated.

Thank you. 

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,461件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anshul

one can check signals with oscilloscope and check iomux

settings: pay attention that sion bit was set.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信