i want to build android for nxp imx8mplus lpddr4 evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i want to build android for nxp imx8mplus lpddr4 evk

391 Views
srinivas_123
Contributor III

i am using nxp imx8mplus lpddr4 evk board.
I am new to Android development and I want to build Android with Android Auto features for my board. Among the following options:

  • Android 14.0.0_2.2.0 (L6.6.36_2.1.0 BSP)

  • 15.0.0_1.2.0_ANDROID_SOURCE

  • NXP i.MX Android proprietary source code for Android 14.0.0_2.2.0

  • 14.0.0_1.2.0_ANDROID_SOURCE

Which one should I download to enable Android Auto support?

0 Kudos
Reply
3 Replies

370 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @srinivas_123 :

 

For Android Auto support.  I would suggest you downloaded the source from below link

https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/android-automotive...

 

It is better to use the latest version.

 

 

Regards

Daniel

0 Kudos
Reply

344 Views
srinivas_123
Contributor III
Hi @danielchen,
I downloaded the tar file
imx-automotive-15.0.0_1.1.0.tar.gz.
Is this the correct tar file to use for Android Auto features?
Actually, my requirement is to port Android Auto on the NXP i.MX8M Plus board. Should I use Automotive Android or regular Android?
0 Kudos
Reply

298 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @srinivas_123 

Yes, it is the right package.

Android automotive is supported by imx8QM and imx8QXPlus. ,  but no by imx8plus.

 

Regards

Daniel

0 Kudos
Reply