i.mx8 I2C bus speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8 I2C bus speed

1,486 Views
chrisrayner
Contributor I

I have a SM bus device running at 100KHz but otherwise the same as an I2C device - is there a way to slow the I2C bus down to be able to use this device?

0 Kudos
Reply
1 Reply

1,328 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chris

this is possible, depending on used part: for i.MX8M one can change

clock frequency in CCM (sect.5.1 Clock Control Module (CCM)),

Table 5-1. Clock Root Table i.MX8MDQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

For i.MX8QM, QX parts using SCFW SCFW Porting Kit

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply