i.mx6ull low ethernet and flexcan performance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6ull low ethernet and flexcan performance

924 次查看
svenalluisetti
Contributor I

Our i.mx6ull board has a poor ethernet and flexcan performance compared to the i.mx6 solo with also one core and the same core frequency.

We are using yocto branch rocko with the mainline Kernel 4.14.87 and the preempr-rt patch.

My question, has the i.mx6ul and the i.mx6ull a lower ethernet (fec) and flexcan performance than the i.mx6 solo ?

Are there any specific things (shared busses) which can explain the lower performance ?

标签 (2)
0 项奖励
回复
1 回复

819 次查看
b36401
NXP Employee
NXP Employee

Please note that i.MX6S has 1Gbit/s Ethernet and i.MX6ULL has 100Mbit/s.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复