i.mx6ull low ethernet and flexcan performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6ull low ethernet and flexcan performance

901 Views
svenalluisetti
Contributor I

Our i.mx6ull board has a poor ethernet and flexcan performance compared to the i.mx6 solo with also one core and the same core frequency.

We are using yocto branch rocko with the mainline Kernel 4.14.87 and the preempr-rt patch.

My question, has the i.mx6ul and the i.mx6ull a lower ethernet (fec) and flexcan performance than the i.mx6 solo ?

Are there any specific things (shared busses) which can explain the lower performance ?

Labels (2)
0 Kudos
Reply
1 Reply

796 Views
b36401
NXP Employee
NXP Employee

Please note that i.MX6S has 1Gbit/s Ethernet and i.MX6ULL has 100Mbit/s.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply