i.mx6ull csi with tw9900

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx6ull csi with tw9900

跳至解决方案
11,966 次查看
tkcheng01
Contributor III

I am working with i.mx6ull csi with tw9900 over bt.656. My camera is NTSC format.

I patch mx6s_capture.c file following guidance(0001-Enable-CSI...) from below link.

imx6ul tw9990 issue 

However, I am unable to get the correct image format. This is what I can capture so far.

Attached herwith the source code on mx6s_capture.c as well as tw9900.c

 

208584_208584.jpgpastedImage_3.jpg

标记 (3)
1 解答
10,344 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tk

had you got it working with adv7180, unfortunately I am not aware

of tw9900 patches. In general one can try with various modes, like pal,

interlace.and progressive modes of sensor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
25 回复数
1,632 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tk

yes subdev (refer to attached files), ADV7180 used PAL, YUV4:2:2(UYVY) interlace output
connected to CSI_DATA[9:2], so one can set similar settings for tw9900.

Best regards
igor

1,632 次查看
tkcheng01
Contributor III

Thanks, I will give it a try and revert back.

0 项奖励
回复
1,632 次查看
tkcheng01
Contributor III

Is some mistake on the code on tw9900.c. After properly initialize SFR in tw9900. It is working now. No changes is require on the code on mx6s_capture.c that I posted at first post.

0 项奖励
回复
1,632 次查看
hoanganh
Contributor III

Hi Tk,

What's SFR in your tw9900. I have same wrong image you.

0 项奖励
回复
10,345 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tk

had you got it working with adv7180, unfortunately I am not aware

of tw9900 patches. In general one can try with various modes, like pal,

interlace.and progressive modes of sensor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复