i.mx6sl, MMPF0200 PMIC question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx6sl, MMPF0200 PMIC question

跳至解决方案
2,486 次查看
kentmeyer
Contributor II

We are planning to use the MMPF0200 with a 3.3V input voltage and suspect

that there will be problems with the SW2 output.

Can SW2 operate with 100% duty, i.e. can the SW2 PMOS be persistently

on if/when SW2 is on?

Can SW2 correctly operate if its output voltage is set equal to its input voltage

(Vsw2=Vsw2in) and Lsw2=0 (a wire in place of the inductor)?

-- Kent

标签 (1)
1 解答
1,869 次查看
vadimaleynikov
Contributor III

Hi,

I understand, thank you.

Unfortunately I could not find the Correct Answer button.

Best regards,

Vadim

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,869 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Kent Meyer,

All the regulators except SWBST are step-down which meaning the input has to be higher than the output. Our recommendation is 250mV headroom for the regulators. So if they need a 3.3V output, the input has to be at least 3.55V for the LDOs and the bucks.

And about your suggestion about to use a wire instead an inductor, SW2 is a Buck Regulator, so the inductor is needed for the LC circuit to filter the pulses to create a smooth DC voltage.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,869 次查看
vadimaleynikov
Contributor III

Hi Jose Reyes,

I work with Kent Meyer and have some follow-up questions.

You explained the regular DCDC operation. But we will have to use it in an unusual way and would like to know will it be correct. Specifically, we would like to know:

1. How
will SW2 operate when its output voltage is set equal to its input voltage (Vsw2=Vsw2in)?

2. Can SW2 operate with 100% duty, i.e. can the SW2 PMOS be persistently on if/when SW2 is on?

Best regards,

Vadim Aleynikov

0 项奖励
回复
1,869 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

[A1] As mentioned, SWx buck regulators are step-down which meaning the input has to be higher than the output.

I just tested it using the MMPF0200 Evaluation board and I can confirm that there is a drop on the SW2 output voltage, when VSW2IN = 3.3V and SW2 output voltage is set to 3.3V, the actual output voltage drops to 3.28V.

[A2] No, SWx buck regulators (switching regulators) operate with a max duty of about 90%, and unfortunately on the MMPF0200 it is not possible to make them work as an LDO (100% duty regulator).


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,870 次查看
vadimaleynikov
Contributor III

Hi,

I understand, thank you.

Unfortunately I could not find the Correct Answer button.

Best regards,

Vadim

0 项奖励
回复