Problem when booting on battery imx233 bga: ERROR_DDI_SD_MULTI_READ_TIMEOUT (0x8020a023)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem when booting on battery imx233 bga: ERROR_DDI_SD_MULTI_READ_TIMEOUT (0x8020a023)

ソリューションへジャンプ
1,285件の閲覧回数
pierreparent
Contributor III

Hi all,

I have a custom board, with an imx233 BGA and 128 Mo of RAM. Everything works almost perfect but one thing.

When I boot form LiPo only I get "HTLCL0x8020a023" (I'm booting form SD BCB). But If I boot form 5V and then disconnect the 5V, the board stays up thanks to the battery.

The thing is I have another custom board with Imx233 LQFP package, with almost same electrical schematics, and very similar layout. And it boots ok from the same battery.

What I've tryed on my imx233 BGA board:

*Add huge capacitance in parallel of  the battery: no change.

*Add huge capacitance in parallel of  3.3v: no change.

*Add 10pf and 100pf capacitors in parallel of the inductor (see imx233 weird DCDC capacitor problems | olimex ): no change

*To replace the inductor by another model: no change.

I'm kind of running out of ideas.

Do you have any hint?

Thanks in advance.

Pierre.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
1,135件の閲覧回数
pierreparent
Contributor III

Ok I've found a solution : Add a 100Uf Tantale trhough hole on 3.3v.

But this is very ugly. I could add as many 22uF as I wanted, it would not change anything.

I'l surprized I get this problem with the BGA version and not the LQFP. Might be a layout issue though.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,136件の閲覧回数
pierreparent
Contributor III

Ok I've found a solution : Add a 100Uf Tantale trhough hole on 3.3v.

But this is very ugly. I could add as many 22uF as I wanted, it would not change anything.

I'l surprized I get this problem with the BGA version and not the LQFP. Might be a layout issue though.

0 件の賞賛
返信