Hi everyone
I have a custom board, and it use spdif interface to output audio.
To enable spdif output feature, i add following red settings to my device tree file.
sound-spdif {
compatible = "fsl,imx-audio-spdif";
model = "imx-spdif";
spdif-controller = <&spdif>;
spdif-out;
};
............
//SPDIF AUDIO OUT
pinctrl_spdif: spdifgrp {
fsl,pins = <
MX6QDL_PAD_GPIO_17__SPDIF_OUT 0x1b0b0
>;
};
....................
&spdif {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_spdif>;
status = "okay";
};
After did this, i can see the sound card use aplay -l,
root@sabre:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: imxspdif [imx-spdif], device 0: S/PDIF PCM snd-soc-dummy-dai-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0
But when i try to play a audio file, it blocked and never return back.
root@sabre:~# aplay /unit_tests/audio8k16S.wav
Playing WAVE '/unit_tests/audio8k16S.wav' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo
when i use gplay, it has the same problem.
In Linux_Reference_Manual.pdf, about the spdif output driver, when use aplay -l,it will be

but, my result is different with snd-soc-dummy-dai-0, not "Playback dit-hifi-0".
I also check the sabreauto reference board,it is also "snd-soc-dummy-dai-0", Why?
I am using the lateset BSP version, fsl-yocto-L4.1.15_1.1.0-ga.
Finally, how can I get spdif output driver work?Qiang_FSL
Thank you.