i.mx6DL cant send data through UART2,3.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6DL cant send data through UART2,3.

2,566件の閲覧回数
ispark
Contributor I

Hello,

Target environment is Android 4.4.2 .

I installed UART2,3 with tested i.mx6Q quad processor without problem.

device is /dev/ttymx1, /dev/ttymx2

But processor MCimx6U5DVM10AC board can not run UART 2, 3 .

So question is I.mx6DL processor UART port has difference with Quad processor?

0 件の賞賛
返信
2 返答(返信)

2,464件の閲覧回数
ispark
Contributor I

thanks for your response.

it was corrected by port pin mapping change.

0 件の賞賛
返信

2,464件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi IS

DL has different than DQ registers addresses, also suggest to

look at attached Porting Guide Chapter 3 Registering a New UART Driver

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信