i.mx6: question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,445件の閲覧回数
jfsimon
Contributor III

Hi,

On our i.mx6DL based design, we have the following IOMUX settings for UART2:

UART2_RX ----> goes to PAD SD4_DAT4

UART2_TX ----> goes to PAD SD4_DAT7

The routing from signal to pad is easy...just set the following MUX registers:

37.3.208 Pad Mux Register (IOMUXC_SW_MUX_CTL_PAD_SD4_DATA4)  ---> ALT2

and

37.3.211 Pad Mux Register (IOMUXC_SW_MUX_CTL_PAD_SD4_DATA7) --->. ALT2

So far so good.

Now, since these two signals  (UART2_RX and UART2_TX) can be driven by different PADs, we need to use a select input register. The problem is that there is a UNIQUE input register for the two signals. Specifically:

IOMUXC_UART2_UART_RX_DATA_SELECT_INPUT (section 37.3.572 in the user manual)   (See picture)

So how can we correctly select the input for these two signals?

Thanks a lot

-jf simon

0 件の賞賛
返信
1 解決策
3,383件の閲覧回数
YS
Contributor IV

Refer to iMX6 Reference Manual 35.2.3 "Daisy Chain". IOMUX_INPUT register is used to select a particular source for a function module input. In this case, RXD of UART2. It is confusing that IOMUX_INPUT provides selection to choose TXD as input source. This is only used for loop-back test. So in your case, configure 110 to select SD4_DAT4 as UART2 RXD input will work fine.

It is more confusing for RTS/CTS, because iMX6 (and iMX5) defines RTS as input and CTS as output, which is usually used in opposite way (in fact iMX28 defines RTS as output, CTS as input).

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,384件の閲覧回数
YS
Contributor IV

Refer to iMX6 Reference Manual 35.2.3 "Daisy Chain". IOMUX_INPUT register is used to select a particular source for a function module input. In this case, RXD of UART2. It is confusing that IOMUX_INPUT provides selection to choose TXD as input source. This is only used for loop-back test. So in your case, configure 110 to select SD4_DAT4 as UART2 RXD input will work fine.

It is more confusing for RTS/CTS, because iMX6 (and iMX5) defines RTS as input and CTS as output, which is usually used in opposite way (in fact iMX28 defines RTS as output, CTS as input).

0 件の賞賛
返信
3,383件の閲覧回数
jfsimon
Contributor III

Hi Yuji,

Thanks a lot for y answer

-jfs

0 件の賞賛
返信