i.mx6 display system problem, black screen.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 display system problem, black screen.

2,234 Views
jack-chen
Contributor I

Hi all:

      I have a question that I'd like to ask you about. After the system is migrated, the display will close after a few minutes (about 5 minutes). The contents displayed after starting up are as follows:

(1) Login

73350185366123060.jpg

 

(2) Backgound picture

510356083276883917.jpg

 

(3) After about 5 minutes, the screen will be black, but the backlight is still on, and the terminal console can control it. Running the display program will not work, and the console will be stuck. The information of my transplanted system is as follows:

  • BSP version: L4.1.15_2.0.0-ga
  • CPU: I.MX6 Dual

      Hope to get your help, thank you!##

Labels (3)
Tags (1)
0 Kudos
Reply
2 Replies

1,804 Views
igorpadykov
NXP Employee
NXP Employee

Hi

one can try to turn off lcd blanking :

LCD turning white after a few minutes 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,804 Views
jack-chen
Contributor I

hello,

   I tried the following command:

echo -e ‘\033[9;0]’ > /dev/tty0
echo -e ‘\033[9;0]’ > /dev/tty1
echo 0 > /sys/class/graphics/fb0/blank
echo 0 > /sys/class/graphics/fb1/blank

It doesn't work. Actually, my console device is tty1 and the framebuff is fb0.

Is there any other way to try it?

0 Kudos
Reply