i.mx6 display system problem, black screen.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6 display system problem, black screen.

2,995件の閲覧回数
jack-chen
Contributor I

Hi all:

      I have a question that I'd like to ask you about. After the system is migrated, the display will close after a few minutes (about 5 minutes). The contents displayed after starting up are as follows:

(1) Login

73350185366123060.jpg

 

(2) Backgound picture

510356083276883917.jpg

 

(3) After about 5 minutes, the screen will be black, but the backlight is still on, and the terminal console can control it. Running the display program will not work, and the console will be stuck. The information of my transplanted system is as follows:

  • BSP version: L4.1.15_2.0.0-ga
  • CPU: I.MX6 Dual

      Hope to get your help, thank you!##

ラベル(3)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,565件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

one can try to turn off lcd blanking :

LCD turning white after a few minutes 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,565件の閲覧回数
jack-chen
Contributor I

hello,

   I tried the following command:

echo -e ‘\033[9;0]’ > /dev/tty0
echo -e ‘\033[9;0]’ > /dev/tty1
echo 0 > /sys/class/graphics/fb0/blank
echo 0 > /sys/class/graphics/fb1/blank

It doesn't work. Actually, my console device is tty1 and the framebuff is fb0.

Is there any other way to try it?

0 件の賞賛
返信