i.mx6 POP packages

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 POP packages

Jump to solution
4,026 Views
JHY
Contributor IV

i.MX 6Dual/6Quad Consumer-PoP Applications Processor

Are POP packages available only in IMX6 Dual or Quad?

Best regards.

Labels (1)
0 Kudos
Reply
1 Solution
3,374 Views
Yuri
NXP Employee
NXP Employee

Hello,

Yes, POP packages available only in IMX6 Dual or Quad, at least right now.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,375 Views
Yuri
NXP Employee
NXP Employee

Hello,

Yes, POP packages available only in IMX6 Dual or Quad, at least right now.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,374 Views
naoum_gitnik
Contributor II

Zdravstvuyte, Igor and Yuri,

Based on the datasheet mentioned, is my understanding correct that the PoP version has no automotive version?

- If you it does, what is its part number, please?

- If not, are there any plans for it?

Zaranee blagodaren, Naoum Gitnik.

[igorpadykov​]

0 Kudos
Reply
3,374 Views
naoum_gitnik
Contributor II

Dear DavidBabin​ and TheAdmiral​,

May you answer this question, please? - Based on the datasheet mentioned above, is my understanding correct that i.MX6 PoP has no automotive version? If not, are there any plans for it?

Sincerely, Naoum Gitnik.

0 Kudos
Reply
3,374 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I have no information about avilabilty and plans regarding automotive version of the PoP. 

Regards,

Yuri.

0 Kudos
Reply