i.mx280 ethernet + nand

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx280 ethernet + nand

ソリューションへジャンプ
1,839件の閲覧回数
yar
Contributor III

Hello,

I am new in I.MX28x family MCU. I want to use NAND (GPMI) + ETHERNET (ENET) together.

I tried to test this configuration in Freescale IO Mux application. Application shows the presence of conflict (screenshot attached).

Whether correctly I understand that in I.MX280 it is impossible to use NAND + ETHERNET simultaneously?

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,711件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Typically you use only one or two NAND chips on designs, so with that you should be fine (GPMI_CE0N, GPMI_CE1N, GPMI_READY0, GPMI_READY1).

If you want to attach additional four NANDs, then yes, you will have some conflicts, but that is not a very typical design.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,712件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Typically you use only one or two NAND chips on designs, so with that you should be fine (GPMI_CE0N, GPMI_CE1N, GPMI_READY0, GPMI_READY1).

If you want to attach additional four NANDs, then yes, you will have some conflicts, but that is not a very typical design.

0 件の賞賛
返信
1,711件の閲覧回数
yar
Contributor III

Thanks for the detailed answer.

0 件の賞賛
返信