i.mx280 ethernet + nand

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx280 ethernet + nand

跳至解决方案
1,761 次查看
yar
Contributor III

Hello,

I am new in I.MX28x family MCU. I want to use NAND (GPMI) + ETHERNET (ENET) together.

I tried to test this configuration in Freescale IO Mux application. Application shows the presence of conflict (screenshot attached).

Whether correctly I understand that in I.MX280 it is impossible to use NAND + ETHERNET simultaneously?

Thanks.

标签 (1)
0 项奖励
回复
1 解答
1,633 次查看
VladanJovanovic
NXP Employee
NXP Employee

Typically you use only one or two NAND chips on designs, so with that you should be fine (GPMI_CE0N, GPMI_CE1N, GPMI_READY0, GPMI_READY1).

If you want to attach additional four NANDs, then yes, you will have some conflicts, but that is not a very typical design.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,634 次查看
VladanJovanovic
NXP Employee
NXP Employee

Typically you use only one or two NAND chips on designs, so with that you should be fine (GPMI_CE0N, GPMI_CE1N, GPMI_READY0, GPMI_READY1).

If you want to attach additional four NANDs, then yes, you will have some conflicts, but that is not a very typical design.

0 项奖励
回复
1,633 次查看
yar
Contributor III

Thanks for the detailed answer.

0 项奖励
回复