i.mx23 connection via ubuntu desktop minicom

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx23 connection via ubuntu desktop minicom

2,387件の閲覧回数
YavuzKaran
Contributor I

Hi,

I'm new to using i.mx23.I have board and its include mini usb.I know mfg tool use this usb port.

First, im using ubuntu 20.04 and connect via usb to i.mx23 board .when check the usb port (lsusb) i can see sigmatel driver.but i can't use minicom.

i want connect imx23 embedded linux and developer software inside.

Maybe i want use rs232 port? but im23 card dont have rs232.

I'm using ubuntu 20.04 and Embedded qt.

Best Regards.

0 件の賞賛
返信
2 返答(返信)

2,378件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi YavuzKaran

 

what board used in the case, if it is based on i.MX233 EVK one can look at

i.MX23 EVK Linux Documentation Bundle

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

Some third parties also develop i.MX233 based boards:

https://www.olimex.com/Products/OLinuXino/iMX233/iMX233-OLinuXino-MICRO/open-source-hardware

 

Best regards
igor

0 件の賞賛
返信

2,374件の閲覧回数
YavuzKaran
Contributor I

Dear Igor ,

Thanks a lot for your quick reply.My product is not evolution board.im using special pcb board and have i.mx23 mcu.I know, my board same character  of i.MX233 EVK board.when load new program for this board, we it like in the link  https://community.nxp.com/t5/i-MX-Processors/How-to-load-image-onto-NAND-flash-at-i-MX23-Evaluation-... .

But i dont have any idea to how to connect via miniusb this board or i.MX233 EVK board.

I will  read the documents you sent.i hope i can find how to connect.

i sent  mfg tool image (loading new program) via attachment

i sent board image 

I will write result.

Thanks a lot for everything.

Regards

0 件の賞賛
返信