imx8mm mini - adding python-opencv to yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mm mini - adding python-opencv to yocto

2,674件の閲覧回数
dudisasson
Contributor I

Hi,

I have added the following to my local.conf file:

 

IMAGE_INSTALL_append = " \

python3   \

python3-numpy   \

python3  - opencv \

opencv \

"

 

but when trying to import cv2 i get the following:

>>> import cv2
Traceback (most recent call last):
File "<stdin>", line 1, in <module>
File "/usr/lib/python3.5/site-packages/cv2/__init__.py", line 8, in <module>
import numpy
File "/usr/lib/python3.5/site-packages/numpy/__init__.py", line 142, in <module>
from . import add_newdocs
File "/usr/lib/python3.5/site-packages/numpy/add_newdocs.py", line 13, in <module>
from numpy.lib import add_newdoc
File "/usr/lib/python3.5/site-packages/numpy/lib/__init__.py", line 8, in <module>
from .type_check import *
File "/usr/lib/python3.5/site-packages/numpy/lib/type_check.py", line 11, in <module>
import numpy.core.numeric as _nx
File "/usr/lib/python3.5/site-packages/numpy/core/__init__.py", line 34, in <module>
from . import umath
SystemError: initialization of umath raised unreported exception

 

Thanks in advance,

Dudi.

 

0 件の賞賛
返信
1 返信

2,658件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信