i.mx patch files in Intel Hex format

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx patch files in Intel Hex format

2,105件の閲覧回数
mickaeltoumi
Contributor III

Would it be possible to provide the Intel .HEX file for this patch here: Patch for the SDK 2010.12 to fix the incorrect polarity when boot mode is set as boot from SD/eMMC o... 

It is currently in .sb format and proprietary to NXP.

If not possible please provide a link to a tool to convert this .sb patch file into Intel Hex format. We are trying to write the patch on the Microchip 24LC128 with some difficulties.

Thank you. 

ラベル(1)
3 返答(返信)

1,893件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mickael T,

These patches are not available in .hex format. I'm investigating if there's a way to convert from one format to the other. I'll let you know if I find something.

Regards,

0 件の賞賛
返信

1,893件の閲覧回数
mickaeltoumi
Contributor III

Hi gusarambula,

I wrote a Python script to format the .sb into the Intel .hex. We mainly got into trouble with the Microchip MPLAD Starter Kit and MPLAB IDE. The IDE does not import raw hex unfortunately (we cannot import .sb).

I will post next week the source of the script and will put a note regarding another programmer that we tested that was able to program raw hex without specific formatting.

1,893件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mickael T,

Thanks for the update.

I just wanted to confirm that I couldn't find the patches in hex format and couldn't find a converter neither. But I'm glad to hear you are making progress! I'm sure the script would be useful to other Community users!

Regards,

0 件の賞賛
返信