i.mx config tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx config tool

583 Views
Robbi
Contributor II

Hi team,

               As a part of DDR exercise test in imx91 custom board. I'm using config tool provided by nxp. I tried it for EVK all DDR tests worked.  Coming to custom board A-55 debug port is changed from LPUART1 to LPUART8. when performing tests, getting error in INFO tab. So, how can I sort this issue and is there any method to test LPDDR4.

I had attached the log information.

Thanks 

Robbi

0 Kudos
Reply
1 Reply

561 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

If you are using a custom board, please confirm that you are using the correct configuration for UART port, PMIC initialization and verify that the board is in serial download mode.

Both debug and USB data cables should be connected to de PC directly without any USB hub.

Best regards.

0 Kudos
Reply