i.mx config tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx config tool

568件の閲覧回数
Robbi
Contributor II

Hi team,

               As a part of DDR exercise test in imx91 custom board. I'm using config tool provided by nxp. I tried it for EVK all DDR tests worked.  Coming to custom board A-55 debug port is changed from LPUART1 to LPUART8. when performing tests, getting error in INFO tab. So, how can I sort this issue and is there any method to test LPDDR4.

I had attached the log information.

Thanks 

Robbi

0 件の賞賛
返信
1 返信

546件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

If you are using a custom board, please confirm that you are using the correct configuration for UART port, PMIC initialization and verify that the board is in serial download mode.

Both debug and USB data cables should be connected to de PC directly without any USB hub.

Best regards.

0 件の賞賛
返信