i.mx 8M Mini: How to power NVCC_SD2 when not using SD2 interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx 8M Mini: How to power NVCC_SD2 when not using SD2 interface?

Jump to solution
2,199 Views
adevries
Contributor V

Hello,

I'm using an i.mx 8M Mini in an application where the SD card interface isn't needed. When I was using this interface previously I had the power pin NVCC_SD2 connected up to a voltage rail that could switch between 1.8V and 3.3V.

According to the Hardware Design Guide, NVCC_SD2 should remain powered even if the interface isn't being used. But since the interface isn't being used and doesn't need to switch between 1.8V and 3.3V, is it acceptable to just power NVCC_SD2 with a standard 1.8V or 3.3V rail? Timing-wise, the rail should just power on and off with all the other NVCC_1V8 and NVCC_3V3 GPIO rails, right?

Labels (1)
0 Kudos
Reply
1 Solution
2,187 Views
igorpadykov
NXP Employee
NXP Employee

yes one can power NVCC_SD2 with just 1.8V. 1.8V or 3.3V does not matter.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
2,192 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexander

 

> Timing-wise, the rail should just power on and off with all the other NVCC_1V8 and NVCC_3V3 GPIO rails, right?

 

yes this is correct.

 

Best regards
igor

0 Kudos
Reply
2,189 Views
adevries
Contributor V

Hi Igor,

Can I power NVCC_SD2 with just 1.8V? Does it matter if I choose 1.8V or 3.3V?

Thanks

0 Kudos
Reply
2,188 Views
igorpadykov
NXP Employee
NXP Employee

yes one can power NVCC_SD2 with just 1.8V. 1.8V or 3.3V does not matter.

 

Best regards
igor

0 Kudos
Reply