i.mx 8M Mini: How to power NVCC_SD2 when not using SD2 interface?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx 8M Mini: How to power NVCC_SD2 when not using SD2 interface?

跳至解决方案
3,235 次查看
adevries
Contributor V

Hello,

I'm using an i.mx 8M Mini in an application where the SD card interface isn't needed. When I was using this interface previously I had the power pin NVCC_SD2 connected up to a voltage rail that could switch between 1.8V and 3.3V.

According to the Hardware Design Guide, NVCC_SD2 should remain powered even if the interface isn't being used. But since the interface isn't being used and doesn't need to switch between 1.8V and 3.3V, is it acceptable to just power NVCC_SD2 with a standard 1.8V or 3.3V rail? Timing-wise, the rail should just power on and off with all the other NVCC_1V8 and NVCC_3V3 GPIO rails, right?

标签 (1)
0 项奖励
回复
1 解答
3,223 次查看
igorpadykov
NXP Employee
NXP Employee

yes one can power NVCC_SD2 with just 1.8V. 1.8V or 3.3V does not matter.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,228 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexander

 

> Timing-wise, the rail should just power on and off with all the other NVCC_1V8 and NVCC_3V3 GPIO rails, right?

 

yes this is correct.

 

Best regards
igor

0 项奖励
回复
3,225 次查看
adevries
Contributor V

Hi Igor,

Can I power NVCC_SD2 with just 1.8V? Does it matter if I choose 1.8V or 3.3V?

Thanks

0 项奖励
回复
3,224 次查看
igorpadykov
NXP Employee
NXP Employee

yes one can power NVCC_SD2 with just 1.8V. 1.8V or 3.3V does not matter.

 

Best regards
igor

0 项奖励
回复