i changed the local.conf, and type bitbake fsl-image-gui, but error generated

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i changed the local.conf, and type bitbake fsl-image-gui, but error generated

1,099件の閲覧回数
jungsaeyim
Contributor I

board : imx6qsabresd

i want to make yocto image with compiler and opencv library.

so i changed local.conf

and type bitbake fsl-image-gui

but error is generated.

i don't know about the error

how can i  do?

thank you

local.conf

local.conf....png

error

빌드 에러1.png

빌드 에러2.png

ラベル(2)
0 件の賞賛
返信
1 返信

878件の閲覧回数
Yuri
NXP Employee
NXP Employee

  I hope the following helps.

Computer Vision on i.MX Processors: Building OpenCV-2.4.X for Freescale's i.MX6 BSP (Yocto)

Re: Yocto and OpenCV for I.MX


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信