i changed the local.conf, and type bitbake fsl-image-gui, but error generated

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i changed the local.conf, and type bitbake fsl-image-gui, but error generated

1,101 Views
jungsaeyim
Contributor I

board : imx6qsabresd

i want to make yocto image with compiler and opencv library.

so i changed local.conf

and type bitbake fsl-image-gui

but error is generated.

i don't know about the error

how can i  do?

thank you

local.conf

local.conf....png

error

빌드 에러1.png

빌드 에러2.png

Labels (2)
0 Kudos
Reply
1 Reply

880 Views
Yuri
NXP Employee
NXP Employee

  I hope the following helps.

Computer Vision on i.MX Processors: Building OpenCV-2.4.X for Freescale's i.MX6 BSP (Yocto)

Re: Yocto and OpenCV for I.MX


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply