How can I program MMPF0100NP to F0 mode in u-boot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I program MMPF0100NP to F0 mode in u-boot?

ソリューションへジャンプ
2,266件の閲覧回数
JHY
Contributor IV

In u-boot console, I excuted 'i2c probe' and confirmed communication with PMIC(0x08 i2c line).

But there are so many parameters that I have a hard time to test.

If there are references for setting PMIC to F0 mode, please tell me how can I get them.

Best regards.

タグ(4)
0 件の賞賛
返信
1 解決策
1,908件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

please refer to

AN4536 AN4536, MMPF0100 OTP Programming Instructions - Application Note

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,909件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

please refer to

AN4536 AN4536, MMPF0100 OTP Programming Instructions - Application Note

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信