i.Mx 8M Nano - Cortex M7 Core frequency Selection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.Mx 8M Nano - Cortex M7 Core frequency Selection

跳至解决方案
2,132 次查看
sergiospader
Contributor II

Good Morning,

As I understand Cortex M7 Core frequency can be configures to 600Mhz or 750Mhz.

Looking at datasheet, the only reference for this configuration is the Voltage Value (0.85 for 600Mhz and 0.95 for 750Mhz)

At my case, I will use 0.85V for 600Mhz.

My question is, how do I configure the internal multipliers of M7 to run at this frequency ? Or I just need to power it with 0.85V and the frequency is consequence.

Thanks

Sergio Spader

0 项奖励
回复
1 解答
2,115 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sergio

 

for configuring M7 frequency one can look at Table 5-1. Clock Root Table (ARM_M7_CLK_ROOT),

Figure 5-2. CCM input clock sources, sect.5.1.8.25 M7 Alternate PLL General Function Control Register

i.MX 8M Nano Applications Processor Reference Manual

In general it is not changed automatically with voltage change.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,116 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sergio

 

for configuring M7 frequency one can look at Table 5-1. Clock Root Table (ARM_M7_CLK_ROOT),

Figure 5-2. CCM input clock sources, sect.5.1.8.25 M7 Alternate PLL General Function Control Register

i.MX 8M Nano Applications Processor Reference Manual

In general it is not changed automatically with voltage change.

 

Best regards
igor

0 项奖励
回复