i.Mx 8M Nano - Cortex M7 Core frequency Selection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.Mx 8M Nano - Cortex M7 Core frequency Selection

ソリューションへジャンプ
2,138件の閲覧回数
sergiospader
Contributor II

Good Morning,

As I understand Cortex M7 Core frequency can be configures to 600Mhz or 750Mhz.

Looking at datasheet, the only reference for this configuration is the Voltage Value (0.85 for 600Mhz and 0.95 for 750Mhz)

At my case, I will use 0.85V for 600Mhz.

My question is, how do I configure the internal multipliers of M7 to run at this frequency ? Or I just need to power it with 0.85V and the frequency is consequence.

Thanks

Sergio Spader

0 件の賞賛
返信
1 解決策
2,121件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sergio

 

for configuring M7 frequency one can look at Table 5-1. Clock Root Table (ARM_M7_CLK_ROOT),

Figure 5-2. CCM input clock sources, sect.5.1.8.25 M7 Alternate PLL General Function Control Register

i.MX 8M Nano Applications Processor Reference Manual

In general it is not changed automatically with voltage change.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,122件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sergio

 

for configuring M7 frequency one can look at Table 5-1. Clock Root Table (ARM_M7_CLK_ROOT),

Figure 5-2. CCM input clock sources, sect.5.1.8.25 M7 Alternate PLL General Function Control Register

i.MX 8M Nano Applications Processor Reference Manual

In general it is not changed automatically with voltage change.

 

Best regards
igor

0 件の賞賛
返信