i.MXRT Manufacturing Boot Enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT Manufacturing Boot Enabled

1,456 Views
sugiyamatoshihi
Contributor V

Hi, 

I have a question about Manufacturing Boot Enabled in Figure 8-1. Boot flow of i.MXRT1050RM rev2.

I suppose Disable SDMMC Manufacture mode fuse is assigned for Manufacturing Boot Enabled, but 

if failed SD boot at that time, where to go?   Waiting correct SD card image forever?

 

Best Regards,

Sugiyama

Labels (1)
0 Kudos
Reply
1 Reply

1,337 Views
Yuri
NXP Employee
NXP Employee

Hello,

  From section 8.11 (SD/MMC manufacture mode) of the i.MX RT1050 RM:
When the internal boot and recover boot (if enabled) failed, the boot goes to the
SD/MMC manufacture mode before the serial download mode.

  That is, the serial download mode is entered, if the SD/MMC manufacture crashes. 


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply