i.MX93 low power boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX93 low power boot

816 Views
WolsYang
Contributor IV

Hi @AldoG ,

    We are tplanning to do i.MX93 low power boot on Yocto 6.12.

    After boot to cm33, is there any way to boot Linux from cm33? 

0 Kudos
Reply
7 Replies

798 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @WolsYang!

Thank you for contacting NXP Support!

 

It is not possible to run Linux on the M core, as it is designed for real-time, low-power tasks and does not have the resources required to support a full Linux operating system.

 

Best regards,
Chavira

0 Kudos
Reply

760 Views
WolsYang
Contributor IV

Hi @Chavira ,

Sorry for unclear description.

I means  when I enable .bin in only m-core at u-boot, after bring up .bin content, u-boot will close (If is not correct, please let me know)

So, after bring up .bin content in only m-core, how can I bring up Linux in a-core?

0 Kudos
Reply

746 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @WolsYang!

 

In the i.MX93, it is possible and even intended for both cores to work together.

Once the M core has booted, you can proceed to boot Linux on the A core. However, you may need to make some adjustments to the device tree, depending on your configuration.

As you know, both cores can access most of the peripherals. Therefore, it’s important to ensure that any peripherals used by the M core are disabled in the device tree for the A core. This prevents resource conflicts and ensures stable operation for both cores.

 

Best Regards!

Chavira

0 Kudos
Reply

738 Views
WolsYang
Contributor IV

Hi @Chavira ,

    Do we have example about this?

    In my understood, after brigng up m-core, u-boot job is done, and will close.

     Then for example after 10 minute, now only m-core is running, how to bring up a-core linux now?

0 Kudos
Reply

718 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @WolsYang!

You can find the complete procedure for working with multiple cores in our i.MX93-EVK examples at the link below:

 

https://github.com/nxp-mcuxpresso/mcux-sdk-examples/tree/main/mcimx93evk/multicore_examples

 

Best regards,
Chavira

0 Kudos
Reply

708 Views
WolsYang
Contributor IV

Hi @Chavira 
    In rpmsg_lite_pingpong_rtos/linux_remote , I see the description

The primary core releases the secondary core from the reset and then the inter-core communication is established

But I didn't see any like bring up a-corc linux code in

rpmsg_lite_pingpong_rtos/linux_remote/main_remote.c

Also in readme-Prepare the Demo

3. Boot Linux BSP to u-boot, and load M core image from SD card to run. (Put the image into SD card before.) => load mmc 1:1 0x80000000 /rpmsg_lite_pingpong_rtos_linux_remote.bin => cp.b 0x80000000 0x201e0000 0x20000 => bootaux 0x1ffe0000 0

4. Append "clk_ignore_unused" in u-boot "mmcargs" env, before booting linux

5 .Boot to linux. Run "echo '7 4 1 7' > /proc/sys/kernel/printk" to change the message level.

 I think is a-core boot first and then use u-boot to enable m-core

0 Kudos
Reply

677 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @WolsYang!

 

to boot Linux in A core you can use the command "boot" in U-boot terminal 

0 Kudos
Reply