i.MX93 ADC External Multiplexer Functionality?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX93 ADC External Multiplexer Functionality?

818 次查看
af_ee
Contributor I

Hello, on page 5247 of the i.MX93 processor reference manual, Rev. 5 dated 05/2024, it states for the ADC:
"Channel selection controls are provided to use internal or external analog multiplexers."
This seems to be the only reference to this functionality within the reference manual.

Is the functionality to drive external analog multiplexers actually supported by the i.MX93 parts or is this perhaps a carry-over from older documentation?
If this functionality is supported, could you please confirm which IO pins can be used to drive the external muxes? Additionally, is the Normal Scan mode able to iterate over the external mux positions as well?

Thank you for your feedback.

0 项奖励
回复
2 回复数

780 次查看
af_ee
Contributor I

Thank you for the reference.
This appears to be documentation describing the input trigger functionality of the ADC to synchronize to an external event. I am asking about the option to output a control signal to an external analog multiplexer to enable additional ADC channels.
You may note this feature was present in prior NXP devices (MA outputs from the block labeled "control mux"): https://community.nxp.com/t5/MPC5xxx/ADC-External-Channels-Usage-in-MPC746C/m-p/665612

0 项奖励
回复

800 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Triggers can be muxed according to the register sent below and the values would be according to the table attached.

JosephAtNXP_0-1727224437526.png

 

JosephAtNXP_1-1727224440917.png

Regards

0 项奖励
回复