i.MX8mm Kernel Lock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8mm Kernel Lock

5,005 Views
okuda
Contributor IV

Hi NXP

I am using yocto kernel version 5.4.3 for the original board.

If you run the qt application in that environment and repeat drawing, the kernel will lock.
When this happens, there will be no debug output.
(Kernel panic logs such as oob and spin_lock are also not output.)

1.During my research, I found ERR050044 in IMX8MM_0N87W.pdf.
   What happens when this phenomenon occurs?
 Does it cause the above phenomenon?

2.Is there a patch for ERR050044?

3.The kernel lock phenomenon does not occur when i.MX 8mm is warmed with a dryer.
 What are the possible factors?
 What kind of research should I do?

Best regards,
Koji Okuda

 

0 Kudos
Reply
8 Replies

4,971 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Sillicon error only can be fixed by next version of chip.Can you confirm your chip number is included in the IMX8MM_0N87W.pdf?

Regards

Zhiming

 

0 Kudos
Reply

4,963 Views
okuda
Contributor IV

1.How can I check the version of chip?
   Is the following content all right?
   /sys/module/galcore/parameters/chipIDs
   cat chipIDs
   4294967295,4294967295,4294967295,4294967295,4294967295,
   4294967295,4294967295,4294967295,4294967295,4294967295


2.The phenomenon does not occur when the cpu temperature is 50 degrees or higher and
   the QT display application is operated.
   /sys/class/thermal/thermal_zone0/temp
   cat temp
   50000

   As the temperature drops from 50 degrees, the time it takes for the Kernel to lock tends to decrease.
   What are the possible factors?

   


   

0 Kudos
Reply

4,953 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Let's check the chip id on top of soc.

Qmiller_0-1651019717830.png

 

0 Kudos
Reply

4,940 Views
okuda
Contributor IV

Hi

The phenomenon does not occur when the cpu temperature is 50 degrees or higher and  the QT display application is operated.
   /sys/class/thermal/thermal_zone0/temp
   cat temp
   50000

As the temperature drops from 50 degrees, the time it takes for the Kernel to lock tends to decrease.

What are the possible factors?

Please give us some advice on the above.

Best Regards
Koji Okuda

0 Kudos
Reply

4,931 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Can you try latest BSP?

If this issue exist in  latest BSP, i can create an internal case.

0 Kudos
Reply

4,926 Views
okuda
Contributor IV

How can I get the latest BSP?
If I can get it, I can try it.

What does "create an internal case." Mean?

0 Kudos
Reply

4,943 Views
okuda
Contributor IV

Hi

The image of SOC has been uploaded.
Can you see this image?

Best regards
Koji Okuda

0 Kudos
Reply

4,991 Views
undertess146
Contributor I
0 Kudos
Reply