i.MX8mm Kernel Lock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8mm Kernel Lock

5,087 次查看
okuda
Contributor IV

Hi NXP

I am using yocto kernel version 5.4.3 for the original board.

If you run the qt application in that environment and repeat drawing, the kernel will lock.
When this happens, there will be no debug output.
(Kernel panic logs such as oob and spin_lock are also not output.)

1.During my research, I found ERR050044 in IMX8MM_0N87W.pdf.
   What happens when this phenomenon occurs?
 Does it cause the above phenomenon?

2.Is there a patch for ERR050044?

3.The kernel lock phenomenon does not occur when i.MX 8mm is warmed with a dryer.
 What are the possible factors?
 What kind of research should I do?

Best regards,
Koji Okuda

 

0 项奖励
回复
8 回复数

5,053 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Sillicon error only can be fixed by next version of chip.Can you confirm your chip number is included in the IMX8MM_0N87W.pdf?

Regards

Zhiming

 

0 项奖励
回复

5,045 次查看
okuda
Contributor IV

1.How can I check the version of chip?
   Is the following content all right?
   /sys/module/galcore/parameters/chipIDs
   cat chipIDs
   4294967295,4294967295,4294967295,4294967295,4294967295,
   4294967295,4294967295,4294967295,4294967295,4294967295


2.The phenomenon does not occur when the cpu temperature is 50 degrees or higher and
   the QT display application is operated.
   /sys/class/thermal/thermal_zone0/temp
   cat temp
   50000

   As the temperature drops from 50 degrees, the time it takes for the Kernel to lock tends to decrease.
   What are the possible factors?

   


   

0 项奖励
回复

5,035 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Let's check the chip id on top of soc.

Qmiller_0-1651019717830.png

 

0 项奖励
回复

5,022 次查看
okuda
Contributor IV

Hi

The phenomenon does not occur when the cpu temperature is 50 degrees or higher and  the QT display application is operated.
   /sys/class/thermal/thermal_zone0/temp
   cat temp
   50000

As the temperature drops from 50 degrees, the time it takes for the Kernel to lock tends to decrease.

What are the possible factors?

Please give us some advice on the above.

Best Regards
Koji Okuda

0 项奖励
回复

5,013 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Can you try latest BSP?

If this issue exist in  latest BSP, i can create an internal case.

0 项奖励
回复

5,008 次查看
okuda
Contributor IV

How can I get the latest BSP?
If I can get it, I can try it.

What does "create an internal case." Mean?

0 项奖励
回复

5,025 次查看
okuda
Contributor IV

Hi

The image of SOC has been uploaded.
Can you see this image?

Best regards
Koji Okuda

0 项奖励
回复

5,073 次查看
undertess146
Contributor I
0 项奖励
回复