i.MX8MQ boot configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8MQ boot configuration

3,071 次查看
bastiann
Contributor I

I am currently updating an existing i.MX7 design to i.MX8M.

The i.MX7 uses QSPI as boot device.

I used MCIMX8M-EVK schematics as reference and found the BOOT_CFG configuration for boot using SD, eMMC, NAND,QSPI and SPINOR. In the reference manual I only find BOOT_CFG for SD/MMC and NAND boot.

Is there no more support for other boot sources than NAND, SD and MMC?

0 项奖励
回复
6 回复数

2,349 次查看
mitchellchen
Contributor I

who can you share how to repeat configure step ? Thank you

0 项奖励
回复

2,349 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  yes, i.MX 8M supports only NAND, SD \ [e]MMC as boot options.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复

2,349 次查看
gary_bisson
Senior Contributor III

Hi YuriMuhin_ng‌,

Then why does the TRM says:

1.6 Primary Boot Options

The i.MX 8M Dual/8M QuadLite/8M Quad supports the following boot devices:

  • NAND FLASH (including SLC and MLC)
  • SDIO / MMC / SDXC
  • eSD 3.0/eMMC 5.0 (fast boot)
  • SPI (serial FLASH)
  • USB
  • QSPI
  • Ethernet (via plug-in mode)

Also in the 6.2.1 Boot Fusemap clearly states SPI NOR as well as QSPI (BOOT_CFG[14]).

Isn't it only the Internal Boot that is limited to NAND and SD/eMMC? Then using Boot from Fuses allows for more options?

Regards,

Gary

0 项奖励
回复

2,349 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 the information of the section 1.6 seem copied from other i.MX devices,

and should be considered as misprints (already reported to the doc team).

Regards,

Yuri.

0 项奖励
回复

2,349 次查看
gary_bisson
Senior Contributor III

Hi Yuri,

Thanks for the clarification. What about the section 6.2.1 Boot Fusemap, is it also a bad copy/paste?

What about Table 6-19 which also mentions SPI NOR?

Thanks,

Gary

0 项奖励
回复

2,349 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 I am afraid, You are right - some boot fuse details contains typo.

Regards,

Yuri.

0 项奖励
回复