i.MX8MQ boot configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MQ boot configuration

2,934件の閲覧回数
bastiann
Contributor I

I am currently updating an existing i.MX7 design to i.MX8M.

The i.MX7 uses QSPI as boot device.

I used MCIMX8M-EVK schematics as reference and found the BOOT_CFG configuration for boot using SD, eMMC, NAND,QSPI and SPINOR. In the reference manual I only find BOOT_CFG for SD/MMC and NAND boot.

Is there no more support for other boot sources than NAND, SD and MMC?

0 件の賞賛
返信
6 返答(返信)

2,212件の閲覧回数
mitchellchen
Contributor I

who can you share how to repeat configure step ? Thank you

0 件の賞賛
返信

2,212件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  yes, i.MX 8M supports only NAND, SD \ [e]MMC as boot options.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信

2,212件の閲覧回数
gary_bisson
Senior Contributor III

Hi YuriMuhin_ng‌,

Then why does the TRM says:

1.6 Primary Boot Options

The i.MX 8M Dual/8M QuadLite/8M Quad supports the following boot devices:

  • NAND FLASH (including SLC and MLC)
  • SDIO / MMC / SDXC
  • eSD 3.0/eMMC 5.0 (fast boot)
  • SPI (serial FLASH)
  • USB
  • QSPI
  • Ethernet (via plug-in mode)

Also in the 6.2.1 Boot Fusemap clearly states SPI NOR as well as QSPI (BOOT_CFG[14]).

Isn't it only the Internal Boot that is limited to NAND and SD/eMMC? Then using Boot from Fuses allows for more options?

Regards,

Gary

0 件の賞賛
返信

2,212件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 the information of the section 1.6 seem copied from other i.MX devices,

and should be considered as misprints (already reported to the doc team).

Regards,

Yuri.

0 件の賞賛
返信

2,212件の閲覧回数
gary_bisson
Senior Contributor III

Hi Yuri,

Thanks for the clarification. What about the section 6.2.1 Boot Fusemap, is it also a bad copy/paste?

What about Table 6-19 which also mentions SPI NOR?

Thanks,

Gary

0 件の賞賛
返信

2,212件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 I am afraid, You are right - some boot fuse details contains typo.

Regards,

Yuri.

0 件の賞賛
返信