i.MX8MP TSN implementation details

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8MP TSN implementation details

跳至解决方案
3,699 次查看
matteo_silotto
Contributor II

Hi support team,

on i.MX8MPlus only one ethernet port supports TSN (ENET2_TSN).

In the EVK reference design, you do not use a PHY with a hardware timestamp nor other additional signals (eg. Start-of-frame detect) from the PHY to the MAC.

So, could you confirm that the TSN implementation on i.MX8MPlus is a pure software or MAC level implementation? And does it not require a specific PHY?

Thanks.

0 项奖励
回复
1 解答
3,648 次查看
Yuri
NXP Employee
NXP Employee

@matteo_silotto 
Hello,

    yes, " the TSN functionality has no dependence on the ethernet PHY used".

Regards,
Yuri.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,679 次查看
matteo_silotto
Contributor II

Hi Yuri,

thanks for the link. I've analyzed it and it explains the software setup for the AVB/TSN demo.

I'm talking about the hardware requirement of the TSN ethernet interface. On the EVK reference schematic there is no hardware difference between EHT1 and ETH2, but only ETH2 supports the TSN.

Could you confirm that the TSN functionality has no dependence on the ethernet PHY used?

Best regards,

Matteo Silotto

0 项奖励
回复
3,692 次查看
Yuri
NXP Employee
NXP Employee

@matteo_silotto 
Hello,

   Customers can refer to the following demo:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/AVB-TSN-demo-on-i-MX8MP/ta-p/1123791

 

Regards,
Yuri.

0 项奖励
回复
3,667 次查看
matteo_silotto
Contributor II

Hi Yuri,

thanks for the link. I've analyzed it and it explains the software setup for the AVB/TSN demo.

I'm talking about the hardware requirement of the TSN ethernet interface. On the EVK reference schematic there is no hardware difference between EHT1 and ETH2, but only ETH2 supports the TSN.

Could you confirm that the TSN functionality has no dependence on the ethernet PHY used?

Best regards,

Matteo Silotto

3,649 次查看
Yuri
NXP Employee
NXP Employee

@matteo_silotto 
Hello,

    yes, " the TSN functionality has no dependence on the ethernet PHY used".

Regards,
Yuri.

0 项奖励
回复