i.MX8MP TSN implementation details

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MP TSN implementation details

ソリューションへジャンプ
3,700件の閲覧回数
matteo_silotto
Contributor II

Hi support team,

on i.MX8MPlus only one ethernet port supports TSN (ENET2_TSN).

In the EVK reference design, you do not use a PHY with a hardware timestamp nor other additional signals (eg. Start-of-frame detect) from the PHY to the MAC.

So, could you confirm that the TSN implementation on i.MX8MPlus is a pure software or MAC level implementation? And does it not require a specific PHY?

Thanks.

0 件の賞賛
返信
1 解決策
3,649件の閲覧回数
Yuri
NXP Employee
NXP Employee

@matteo_silotto 
Hello,

    yes, " the TSN functionality has no dependence on the ethernet PHY used".

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,680件の閲覧回数
matteo_silotto
Contributor II

Hi Yuri,

thanks for the link. I've analyzed it and it explains the software setup for the AVB/TSN demo.

I'm talking about the hardware requirement of the TSN ethernet interface. On the EVK reference schematic there is no hardware difference between EHT1 and ETH2, but only ETH2 supports the TSN.

Could you confirm that the TSN functionality has no dependence on the ethernet PHY used?

Best regards,

Matteo Silotto

0 件の賞賛
返信
3,693件の閲覧回数
Yuri
NXP Employee
NXP Employee

@matteo_silotto 
Hello,

   Customers can refer to the following demo:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/AVB-TSN-demo-on-i-MX8MP/ta-p/1123791

 

Regards,
Yuri.

0 件の賞賛
返信
3,668件の閲覧回数
matteo_silotto
Contributor II

Hi Yuri,

thanks for the link. I've analyzed it and it explains the software setup for the AVB/TSN demo.

I'm talking about the hardware requirement of the TSN ethernet interface. On the EVK reference schematic there is no hardware difference between EHT1 and ETH2, but only ETH2 supports the TSN.

Could you confirm that the TSN functionality has no dependence on the ethernet PHY used?

Best regards,

Matteo Silotto

3,650件の閲覧回数
Yuri
NXP Employee
NXP Employee

@matteo_silotto 
Hello,

    yes, " the TSN functionality has no dependence on the ethernet PHY used".

Regards,
Yuri.

0 件の賞賛
返信