i.MX8MP Deinterlacing – Low FPS issue on 5.15 (kirkstone) BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MP Deinterlacing – Low FPS issue on 5.15 (kirkstone) BSP

66件の閲覧回数
Baha_Yenioglu
Contributor II

Hello,

We are experiencing the same issue as described in the following post:
Deinterlacing with i.MX8MP – FPS Drop Issue with TW9992

We are currently using the 5.15 (kirkstone) BSP, and with the deinterlacing patches applied, the streaming frame rate is still quite low (around 15 FPS). In the referenced post, I noticed that NXP technical support mentioned the frame rate was improved to 25 FPS in the latest BSP release.

My questions are:

  • What were the main changes that led to this FPS improvement?

  • Is it possible to integrate these changes into the 5.15 (kirkstone) release we are currently using?


    Thanks,

    Best Regards.

0 件の賞賛
返信
1 返信

24件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

The performance improvement could relate to driver in drivers/staging/media/imx and gstreamer plugin. Therefore, if you need to upgrade, it is best to upgrade both the application layer and the driver layer simultaneously.


Best Regards,
Zhiming

0 件の賞賛
返信