i.MX8MP Custom Board Driver for Peripherals

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8MP Custom Board Driver for Peripherals

跳至解决方案
652 次查看
Wobaffet
Senior Contributor I

Hello,

We are bringing up our custom board, we've configured DDR and we booted with a minimal linux. For upcoming processes, how should we enable drivers, for example we are using a Audio Codec from TI. It has a driver inside the linux. How should we enable it? What is the best way to do it. Also how can we enable peripherals which don't included in linux but developed by some 3rd party developers?

Thank you in advance!

Best Regards.

0 项奖励
回复
1 解答
642 次查看
joanxie
NXP TechSupport
NXP TechSupport

the best way is that you need check if kernel dts file includes this codec already, if yes, you just set the status to OK, if no you need add it to the dts file, and if current bsp already have this peripherals driver already, you need to double check if current menuconfig already enable it or not

在原帖中查看解决方案

0 项奖励
回复
1 回复
643 次查看
joanxie
NXP TechSupport
NXP TechSupport

the best way is that you need check if kernel dts file includes this codec already, if yes, you just set the status to OK, if no you need add it to the dts file, and if current bsp already have this peripherals driver already, you need to double check if current menuconfig already enable it or not

0 项奖励
回复