i.MX8MP Custom Board Driver for Peripherals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MP Custom Board Driver for Peripherals

Jump to solution
1,340 Views
Wobaffet
Senior Contributor I

Hello,

We are bringing up our custom board, we've configured DDR and we booted with a minimal linux. For upcoming processes, how should we enable drivers, for example we are using a Audio Codec from TI. It has a driver inside the linux. How should we enable it? What is the best way to do it. Also how can we enable peripherals which don't included in linux but developed by some 3rd party developers?

Thank you in advance!

Best Regards.

0 Kudos
Reply
1 Solution
1,330 Views
joanxie
NXP TechSupport
NXP TechSupport

the best way is that you need check if kernel dts file includes this codec already, if yes, you just set the status to OK, if no you need add it to the dts file, and if current bsp already have this peripherals driver already, you need to double check if current menuconfig already enable it or not

View solution in original post

0 Kudos
Reply
1 Reply
1,331 Views
joanxie
NXP TechSupport
NXP TechSupport

the best way is that you need check if kernel dts file includes this codec already, if yes, you just set the status to OK, if no you need add it to the dts file, and if current bsp already have this peripherals driver already, you need to double check if current menuconfig already enable it or not

0 Kudos
Reply