i.MX8MM as USB Slave device.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MM as USB Slave device.

ソリューションへジャンプ
3,067件の閲覧回数
vignesh-baskaran
Contributor III

Hi, 

We are trying to imx8mm-evk as peripheral for PC to EVK communication.

We were unable to see the device on both PC and EVK side.

But it can able to detect pendrive.(evk as host)

 

Any suggestions on this one?

 

 

Thanks.

0 件の賞賛
返信
1 解決策
2,987件の閲覧回数
dtony
Contributor III

You need gadget driver. 

here is the test of mass storage gadget test. 

The i.MX8MM evk become a storage.  boot fat partition can be read by window. rootfs ext4 cannot. 

If you connect to a Linux, you can see both partitions. 

If you want you can test usb serial(uart) gadget, usb ethernet gadget.

Untitled.png

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,988件の閲覧回数
dtony
Contributor III

You need gadget driver. 

here is the test of mass storage gadget test. 

The i.MX8MM evk become a storage.  boot fat partition can be read by window. rootfs ext4 cannot. 

If you connect to a Linux, you can see both partitions. 

If you want you can test usb serial(uart) gadget, usb ethernet gadget.

Untitled.png

0 件の賞賛
返信
2,969件の閲覧回数
vignesh-baskaran
Contributor III

Hi @dtony,

Thanks it works !

0 件の賞賛
返信
3,033件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @vignesh-baskaran ,

 

It make me thing that the USB1_VBUS line was not correctly asserted, could you please check it?

 

Best regards!

0 件の賞賛
返信