i.MX8MM Support Camera RAW10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MM Support Camera RAW10

7,603件の閲覧回数
tcchoub
Contributor I

Dear Sir,

I can display camera RAW8 (640x480) on i.MX8MM normally.

(by "gst-launch-1.0 -v v4l2src device=/dev/video0 ! bayer2rgb ! autovideosink")

But, when I display RAW10 (640x480), the image will be very noisy.

(Please see the attached file to display raw10 black-white color-bar)

The warnning message (by --gst-debug-level=3) is below:

--------------------------------------------------------------------------------------------------

 0:00:00.525927500 3957 0x2fcb84a0 WARN v4l2bufferpool gstv4l2bufferpool.c:794:gst_v4l2_buffer_pool_start:<v4l2src0:pool:src> Uncertain or not enough buffers, enabling copy threshold

0:00:01.029631125 3957 0x2fcb84a0 WARN waylandsink wlwindow.c:174:gst_wl_window_new_internal: init surface_state fail, fallback to scale=1 fullscreen (1920x1048)
0:00:01.031814500 3957 0x2fcb8940 WARN v4l2src gstv4l2src.c:692:gst_v4l2src_query:<v4l2src0> Can't give latency since framerate isn't fixated !

--------------------------------------------------------------------------------------------------

I found the following discussion of  "Support Camera RAW10" in NXP Community:

-- Camera Support For RAW10 Format 

-- Ov5640 camera RAW10 format on i.MX8MM  

-- Confirmed support for RAW12 through 4-lane CSI-2 sensor on i.MX8M? 

Currently, I modify "mx6s_capture.c" as below:

(a).

static struct mx6s_fmt formats[] = {

.......................................

{
.name = "RAWRGB10 (SBGGR10)",
.fourcc = V4L2_PIX_FMT_SBGGR10,
.pixelformat = V4L2_PIX_FMT_SBGGR10,
.mbus_code = MEDIA_BUS_FMT_SBGGR10_1X10,
.bpp = 2,
}

}

(b).

witch (csi_dev->fmt->pixelformat) {
.................................................
case V4L2_PIX_FMT_SBGGR10:
width = pix->width * 2;
break;
.................................................
}

(c).

cr1 = csi_read(csi_dev, CSI_CSICR1);
cr1 &= ~BIT_GCLK_MODE;
cr1 |= BIT_PIXEL_BIT; 
csi_write(csi_dev, cr1, CSI_CSICR1);

(d). 

switch (csi_dev->fmt->pixelformat) {

...........................................
PIX_FMT_SBGGR10:
cr18 |= BIT_MIPI_DATA_FORMAT_RAW10;
break;
............................................
}

Does anyone can help us ?  Our Question:

1). Have any configuration I need to modify to support RAW10 ? 

2). For RAW10 data arranged(i.e. 16-bit with actual data in the 10 high bits), does any code/configuration we need to modify ? 

Many thanks for your help.

Sincerely,

TC.Chou

タグ(1)
4 返答(返信)

5,926件の閲覧回数
btarnowski
Contributor III
0 件の賞賛
返信

7,043件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi [email protected] ,

Can you please provide the below information:

1.  Are you using gstreamer1.0-plugins-good? if yes, then can you please provide the steps which you have used to add "bayer2rgb"?

2.  Which yocto version you are using?

Regards,

Radhika Somaiya.

0 件の賞賛
返信

7,043件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

if you can display raw8 but failed with raw10, pls check if you set your sensor correct, another customer used OV725 has the same issue, he fixed this issue as below:

" it was a camera configuration issue. Our camera was sending the one line of meta data as pixel data instead of the correct mipi meta data packet type (0x12)."

6,014件の閲覧回数
udhayamoorthi
Contributor II

same issue here.. i can able to stream or capture using raw8 but can't able to stream or capture on raw10 with imx8mm..am i missing something? i have followed some thread to add raw 10 but it didn't helped me..

0 件の賞賛
返信