i.MX8MM PWM Issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MM PWM Issues

Jump to solution
2,100 Views
oprata
Contributor II

Hello Folks,

I trying to setup PWM pin on imx8mm but I doesn't work. At my configuration, I add those lines

&pwm1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm1>;
status = "okay";
};

&pwm2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm2>;
status = "okay";
};
 

 

and

pinctrl_pwm1: pwm1grp {
fsl,pins = <
MX8MM_IOMUXC_I2C4_SDA_PWM1_OUT 0x16
>;
};

pinctrl_pwm2: pwm2grp {
fsl,pins = <
MX8MM_IOMUXC_I2C4_SCL_PWM2_OUT 0x16
>;
};

 

on dts file and I include this line

CONFIG_PWM=y
CONFIG_PWM_IMX_TPM=y 

 

on my *_deconfig file. After bake my image with Yocto builder and download the image for my Single Board Computer I saw at /sys/class/pwm folder this

lrwxrwxrwx 1 root root 0 Apr 28 2022 pwmchip0 -> ../../devices/platform/soc@0/30400000.bus/30660000.pwm/pwm/pwmchip0
lrwxrwxrwx 1 root root 0 Apr 28 2022 pwmchip1 -> ../../devices/platform/soc@0/30400000.bus/30670000.pwm/pwm/pwmchip1

But on the /dev folder I didn't see the nodes for pwmchip0 and pwmchip1. Does anyone could give me a tips what I missing or what do I mistake?

Thanks in advance.

Labels (1)
0 Kudos
Reply
1 Solution
2,052 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @oprata 

There is no missing or mistake in your configuration. As you can see the pwmchipN existing in the /sys/class/pwm folder which is defined by Kernel.

 

Best regards

Harvey

View solution in original post

0 Kudos
Reply
1 Reply
2,053 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @oprata 

There is no missing or mistake in your configuration. As you can see the pwmchipN existing in the /sys/class/pwm folder which is defined by Kernel.

 

Best regards

Harvey

0 Kudos
Reply