imx8qxp 双屏显示的应用问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp 双屏显示的应用问题

3,515 Views
baijinlong
Contributor III

各位:

        我们基于NXP kernel-4.14.98版本开发了demo板,目前已经成功驱动2个LVDS屏幕,可以通过鼠标将QT应用拖拽到不同的屏幕上显示。为了实现双屏同显和双屏异显,我们参考了imx6的配置方法,但imx8qxp显示框架为drm,imx6的方法在imx8上无效。目前我们遇到的问题:

        1.双屏异显:在命令行模式下,我们要如何配置才能让2个屏幕显示指定的内容?比如,LVDS-1上显示QT-APP-1应用程序,LVDS-2上显示QT-APP-2应用程序。

        2.双屏同显:如何配置才能实现双屏同显?

Yocto工程为4.14.98,文件系统采用NXP编译的固件,图形后端/桌面为wayland/weston.

0 Kudos
4 Replies

3,340 Views
joanxie
NXP TechSupport
NXP TechSupport

try to use the Qt5_Cinematics is under /usr/share/cinematicexperience-1.0/
you have to click with the mouse at the destination monitor, then run the cinematics with &, click with the mouse at the second display, and run the cinematic again.

0 Kudos

3,340 Views
baijinlong
Contributor III

感谢回复。

采用键鼠的方式我知道如何实现双屏异显;

但我们更关心的是如何配置wayland/weston桌面,使得能够不用键鼠,而是使用命令终端实现双屏同显和双屏异显?

0 Kudos

3,340 Views
joanxie
NXP TechSupport
NXP TechSupport

if you playback the video, you can use gstreamer to display different video to the different display, but if you display weston desktop, you need to use mouse

0 Kudos

1,539 Views
mengfei
Contributor III

hello ,

    please tell me how to use command to display different video to different display. i have seach for some messenge on internet ,but always use overlaysink,but in I.MX8M Plus BSP it was not exist.

0 Kudos