i.MX8MM EVK Cannot find i2c devices once Android is started

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MM EVK Cannot find i2c devices once Android is started

1,194件の閲覧回数
martindenion
Contributor II

I'm trying to use the GPIO expander of the i.MX8MM EVK board (OS android) from the user space.
From U-Boot, on the I2C-2 bus, I can find a device at address 20 but once Android has started, I cannot find any i2c device with i2cdetect.

From U-Boot:

u-boot=> i2c dev 0
Setting bus to 0
u-boot=> i2c probe
Valid chip addresses:  25
u-boot=> i2c dev 1
Setting bus to 1
u-boot=> i2c probe
Valid chip addresses:  00 14 50 52 72 73
u-boot=> i2c dev 2
Setting bus to 2
u-boot=> i2c probe
Valid chip addresses:  20

 

From userspace:

evk_8mm:/ # i2cdetect -y 0
i2cdetect: /dev/i2c-0: No such file or directory
evk_8mm:/ # i2cdetect -y 1
i2cdetect: /dev/i2c-1: No such file or directory
evk_8mm:/ # i2cdetect -y 2
i2cdetect: /dev/i2c-2: No such file or directory

 

0 件の賞賛
返信
1 返信

1,187件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信