i.MX8MM Chromium Build Crash in Yocto imx-4.14.78-1.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8MM Chromium Build Crash in Yocto imx-4.14.78-1.0.0

跳至解决方案
1,696 次查看
thom
Contributor II

Hay Guys, 

i currently try to build a yocto and got the following Problem: 

- If i Compile the Image with xwayland and without Chrome all is fine

- If i try to make a Image with Chrome-Ozone-Wayland it crash after 70% while "do_compile" 
- If i try to Build the Chromium standalone "bitbake chrome-ozone-wayland" ti allso stucks at 70%

Can anyone help to fix this Issue? 

0 项奖励
回复
1 解答
1,362 次查看
thom
Contributor II

Hay, 

so the issue was "to low memory". My Build PC have 8 Gbyte, i got the error with this.  And with 16GByte all is fine 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,363 次查看
thom
Contributor II

Hay, 

so the issue was "to low memory". My Build PC have 8 Gbyte, i got the error with this.  And with 16GByte all is fine 

0 项奖励
回复
1,362 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Thomas Stockklauser,

Does this problem still continue?

Would you please provide more information on which BSP you are using?

Regards,

0 项奖励
回复