i.MX8M mini TMU 2 points DC offset value confirmation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M mini TMU 2 points DC offset value confirmation

ソリューションへジャンプ
1,888件の閲覧回数
Tori-san
Contributor III
Hello, According to the IMX8MMRM.pdf clause 5.4.6, hardware will do 1 point calibration (software can do 2 points calibration). In this ase, are the temperature values at these 2 points eFUSE in the product test process? Is there some register like OCOTP_ANA1 of IMX6? How to confirm TE1 at 25 Celsius, and TE2 at 85 Celsius? In other words, how to calculate DC offset at room temperature(25 Celsius) and high temperature(85 Celsius)?
0 件の賞賛
返信
1 解決策
1,875件の閲覧回数
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

  I've sent  some comments directly.

Regards,
Yuri.

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,843件の閲覧回数
Tori-san
Contributor III

Hi Yuri,

Thank you for your reply.

I was able to confirm the value stored in the fuses at address 0x3035_04F0 (bank 3 word 3).

[7:0] was the raw value at 25C(TE1) and [15:8] was the raw value at 85C(TE2).

BTW, Register OCOTP_HW_OCOTP_ANA1 (0x3035_04F0) is explained in RM(Rev.2 08/2019),
but it was deleted in RM(Rev.3 11/2020). What is the reason?

Best regards,

Tori-san.

1,876件の閲覧回数
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

  I've sent  some comments directly.

Regards,
Yuri.

 

0 件の賞賛
返信
1,855件の閲覧回数
Tori-san
Contributor III
Hi Yuri, I appreciate your reply for questions I posted. The question has become almost clear and I sent some comment as reply directly.