i.MX8M mini TMU 2 points DC offset value confirmation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8M mini TMU 2 points DC offset value confirmation

跳至解决方案
2,858 次查看
Tori-san
Contributor III
Hello, According to the IMX8MMRM.pdf clause 5.4.6, hardware will do 1 point calibration (software can do 2 points calibration). In this ase, are the temperature values at these 2 points eFUSE in the product test process? Is there some register like OCOTP_ANA1 of IMX6? How to confirm TE1 at 25 Celsius, and TE2 at 85 Celsius? In other words, how to calculate DC offset at room temperature(25 Celsius) and high temperature(85 Celsius)?
0 项奖励
回复
1 解答
2,845 次查看
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

  I've sent  some comments directly.

Regards,
Yuri.

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,813 次查看
Tori-san
Contributor III

Hi Yuri,

Thank you for your reply.

I was able to confirm the value stored in the fuses at address 0x3035_04F0 (bank 3 word 3).

[7:0] was the raw value at 25C(TE1) and [15:8] was the raw value at 85C(TE2).

BTW, Register OCOTP_HW_OCOTP_ANA1 (0x3035_04F0) is explained in RM(Rev.2 08/2019),
but it was deleted in RM(Rev.3 11/2020). What is the reason?

Best regards,

Tori-san.

2,846 次查看
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

  I've sent  some comments directly.

Regards,
Yuri.

 

0 项奖励
回复
2,825 次查看
Tori-san
Contributor III
Hi Yuri, I appreciate your reply for questions I posted. The question has become almost clear and I sent some comment as reply directly.