i.MX8M mini TMU 2 points DC offset value confirmation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M mini TMU 2 points DC offset value confirmation

Jump to solution
1,875 Views
Tori-san
Contributor III
Hello, According to the IMX8MMRM.pdf clause 5.4.6, hardware will do 1 point calibration (software can do 2 points calibration). In this ase, are the temperature values at these 2 points eFUSE in the product test process? Is there some register like OCOTP_ANA1 of IMX6? How to confirm TE1 at 25 Celsius, and TE2 at 85 Celsius? In other words, how to calculate DC offset at room temperature(25 Celsius) and high temperature(85 Celsius)?
0 Kudos
Reply
1 Solution
1,862 Views
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

  I've sent  some comments directly.

Regards,
Yuri.

 

View solution in original post

0 Kudos
Reply
3 Replies
1,830 Views
Tori-san
Contributor III

Hi Yuri,

Thank you for your reply.

I was able to confirm the value stored in the fuses at address 0x3035_04F0 (bank 3 word 3).

[7:0] was the raw value at 25C(TE1) and [15:8] was the raw value at 85C(TE2).

BTW, Register OCOTP_HW_OCOTP_ANA1 (0x3035_04F0) is explained in RM(Rev.2 08/2019),
but it was deleted in RM(Rev.3 11/2020). What is the reason?

Best regards,

Tori-san.

1,863 Views
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

  I've sent  some comments directly.

Regards,
Yuri.

 

0 Kudos
Reply
1,842 Views
Tori-san
Contributor III
Hi Yuri, I appreciate your reply for questions I posted. The question has become almost clear and I sent some comment as reply directly.